P-300 programmer/controller simulation
Just click on the 'screen' as if you were operating an ESPEC chamber to explore all this controller can do.
Constant Setup Details: Equipment
Sometimes during constant mode operation, the refrigeration needs to
be set manually (usually just on or off)
Time signals allow external devices to be activated when the chamber
is running this constant setup.
There are additional settings for Time Signals, Others, and Option across the bottom of the screen.