Typical Walk-in Configuration

This is a pretty typical walk-in system. The door and console could be installed on the end of the chamber or on the opposite side, if desired. The conditioning MAP on the right side is our largest type, in this case containing 30-hp cascade refrigeration system, suitable for large loads and/or fast temperature cycling.

RSS 2.0Latest News