In order to support a vehicle, the chamber’s insulated floor must be specially constructed. ESPEC has a unique system of multi-layer supports that easily supports the weight while providing good insulation and thermal integrity. The floor is thicker than usual, and has weld-marks on the surface as part of this special construction. Due to the large size of this chamber, this floor ships in two pieces.
This view also shows a black hose used to connect to the automobile’s exhaust.