Alternate view of infrared test

From this view you can see the plenum at the back of the chamber that takes up the whole width. There are three blower wheels in the plenum creating 10,000 CFM, coming out the two upper grilles.

From this view you can see the sensor wires more clearly. Also note that the lighting is angled to ensure even coverage of the sides of the vehicle.

RSS 2.0Latest News

Product types

Industry Applications

Resources and articles

Customer Support

About ESPEC